AXIS#.HOME.MODE

Description

AXIS#.HOME.MODE specifies the homing procedure of the drive. The homing modes available in the drive are summarized in the following table.

Mode Description

0

Current position

1

Find limit switch

2

Find limit switch then find zero angle

3

Find limit switch then find index

4

Find home switch

5

Find home switch then find zero angle

6

Find home switch then find index

7

Find zero angle

8

Find end stop

9

Find end stop then find zero angle

10

Find end stop then find index

11

Find index signal, without any precondition

12

Find home switch, including end stop detection

13 Absolute Mode - Use Feedback Position
14 Reserved
15 Find next feedback zero position
16 Find home switch using dual edges

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

N/A

Range

0 to 15

Default Value

0

Data Type

Integer

See Also

AXIS#.HOME.MOVE
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
AXIS1.HOME.MODE

5008h

02h

Unsigned16

-

-

Read/Write

No

AXIS2.HOME.MODE

5108h

02h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.MODE

6107

17DB

Unsigned16

Read/Write

-

AXIS2.HOME.MODE

71643

117D

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.MODE

6107

Unsigned16

Read/Write

-

Related Topics

Homing